Tool/software:
Hi
We are using the UC1825J as a PWM controller for aircraft lighting. The UC1825 is controlling switching transistors and transformers to use the aircraft power source of 20V to 31V. The output is 28V +/-3V. What is the range of regulation of the UC1825J? Will the output remain in regulation when the DC input drops to 20V? The main output is divided down to 2.5V and compared with a fixed +2.5V reference
thanks
Stan