This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172: BQ25172DSG TMR Resistor

Part Number: BQ25172

Tool/software:

您好

觀看BQ25172DSG相關資料,了解透過TMR Pin Detection resistor  seting 來決定充電時間以及透過BATTERY CHARGER PROTECTION:1.7V 進行過電壓保護。

目前使用專案使用Ni-MH cell 900mA 2串兩並。

預設TMR:15Kohm(12hours)、VSET:27Kohm、ISET:1.5Kohm。

請問這樣的設定是否有問題,比較想確認的是在TMR 設定是建議18kohm 或是15kohm ?

以及請提供關於鎳氫電池耐受過度充電的測試數據?

Hello

View BQ25172DSG related information to learn how to determine the charging time through TMR Pin Detection resistor setting and over-voltage protection through BATTERY CHARGER PROTECTION:1.7V.

The  project uses Ni-MH cell 900mA 2 series 2 parallel batteries.

Preset TMR: 15Kohm (12 hours), VSET: 27Kohm, ISET: 1.5Kohm.

Is there any problem with this setting? I would like to confirm whether 18kohm or 15kohm is recommended for TMR setting?

And please provide test data on NiMH battery's tolerance to overcharge?

  • Hello

    Preset TMR: 15Kohm (12 hours), VSET: 27Kohm, ISET: 1.5Kohm.

    Is there any problem with this setting? I would like to confirm whether 18kohm or 15kohm is recommended for TMR setting?

    ISET 1.5k ohm, this is 200mA charge current.  For 900mAh X 2 for battery configuration, TMR setting of 10 hours would be minimum, 12 hours would be better setting.

    VSET of 27k is good.

    And please provide test data on NiMH battery's tolerance to overcharge?

    What battery manufacture are you using and can you share data sheet?

  • 請提供鎳氫電池耐過充性的測試數據?
  • Hello

    請提供鎳氫電池耐過充性的測試數據?---- Please provide test data on the over-charge resistance of the NiMH battery? 

    What battery manufacture are you using and can you share data sheet?