This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95430: Current design derating

Part Number: CSD95430


Tool/software:

Hi TI Team,

Base on the spec as below picture showing, there are two specs for the output current, the peak continuous current is 90A, and DC(RMS) current is 40A.

1. We want to know how to do the current derating for this power stage?

2.  Can it replace the part TDA21590 from Infineon, which max average load curent is 90A.