This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM828303: what is DCR value of TPSM828303?

Part Number: TPSM828303

Tool/software:

Hi team,

May I know DCR value of TPSM828303 inductor? Is DCR the same for both two different package(RDS/ VCB)?

Regards,

Ben

  • Hello Ben,

    Thanks for reaching out in E2E.

    The DCR value TPSM828303ARDS inductor is typically 26 mΩ.

    The DCR value is different for the two package options (please refer to the specified RDP value in section 6.6 of the datasheet).

    Btw: the inductance value is also different for the two package options (see section 8.1 in the datasheet).

    Best regards,

    Andreas.