Tool/software:
I am trying to activate cell balancing on the BQ76905EVM board.
The jumpers have been configured to act as a 3 cell battery and 12.6V is applied to the Battery inputs.
In Battery Management Studio, I can read registers and write certain commands, such as switching to UNSEALED.
However I need help with the commands and subcommands.
What register should the 0x0083 command to activate cell balancing be written to?
I have attempted [10 00 83] and [10 00 00 83].
I can not find a register address list/map in the technical reference manual nor datasheet?
Is there a resource to see all the register addresses and possible commands?
Thank you.
Regards,
John