Other Parts Discussed in Thread: BQ25798, TPS25751, TPS25730EVM, BQ25758, , TPS26750
Tool/software:TPS25751 、BQ25798
I prepared two batteries (single-cell 4.2V each) for a simple charging test. I’ve already switched to JP1 and used the following bin file for the setup. However, I’m observing different results depending on the adapter, even with the same settings.
Specifically, at 20V, many adapters only output 0.08A of current.
Later, I tested each adapter by using it to charge a laptop, and I found that at 20V, the current could reach 2.3A to 2.4A. This leads me to believe that there is no issue with the adapters themselves.
I’m not sure what could be causing this behavior.
Could someone help clarify this issue?