Part Number: TPS63900
Other Parts Discussed in Thread: TPS61094, TPS61033, TPS61022
Tool/software:
Good morning,
I am working on a design of a NB-IOT product with a bobbin battery (LI-SOCL2) + ELDC supercapacitor (1.5F)
Vin = 2.5 - 3.8V
Vout NB-IOT = 4.0V
Vout Peripherals = 3.3V
The battery (LS33600) may supply a maximum continuous current of 250mA.
The capacitor is therefore there to absorb the current peaks.
My tests have shown that 100mA current limit is too little for an NB-IOT transmission.
Do you have a good replacement for the TPS63900.
I want to see if this is possible before I put the TPS63900 in parallel.
This question is similar, but I only have 1 battery and not 2 in series
e2e.ti.com/.../pulse-power-supply-for-a-lte-modem-with-a-li-socl2-battery