Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi,
Our battery manufacturer is currently using BQ28Z610-R1 in the design.
When our device is booted up at -20 degree, during boot up process,SOC will report 0%, because the battery voltage drop under 3.4V. Then, system will shutdown due to SOC 0%.
After then, because the SOC is 0% already, device will not be booted up even if the temperature goes up 20 degree and battery voltage is above 3.8V.
The devices still needs to be charged to let gauge to recalculate SOC from 0%.
Does it have any way to let SOC value to return to normal value when the temperature become warm except charging?Send some commands to reset SOC during boot up??
For the reset command 0x0041, it had been tried in BQstudio tool, it may not be worked because the battery voltage will be cut off for a while during reset.
Please help to give some advice for this scenario.
Thanks.
Ian Lee.