Tool/software:
As per our product requirement we need to use the eFuse part TPS259474ARPWR in parallel configuration. The concern here is that if the current is unevenly distributed between the two parts and any one of the two part tries to deliver more than the rated output current (5.5A) then both the parts will shut off even though the total current is within the limit of cumulative output current of both parts (5.5 + 5.5 = 11A). So it is essential to know that the difference in output current between both the parts will not be significant.
What is the maximum delta in current we can expect from this parallel operation, considering identical routing for both the ICs?