This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65224-Q1: Regarding TPS6522312WRAHRQ1 datasheet

Part Number: TPS65224-Q1
Other Parts Discussed in Thread: TPS65223-Q1, TPS65223, TPS65224

Tool/software:

In our project we are going to use this PMIC TPS6522312WRAHRQ1 , please share us the datasheet as we are not able to find on online.

  • Hi,

    you can find all latest documents in the secure folder for which you can request access here.

    The relevant documents for this device are the data sheet for TPS65223-Q1 (still in draft phase since this device hasn't been released yet) and one of the user's guides for TPS6522312. There are multiple user's guides for this device since this one device supports multiple PDNs (power distribution networks) through external resource selection (pull down resistors and voltage monitors). 

    If you want to check the latest information in the data sheet you can use the TPS65224 data sheet since that has been released to market already. The only difference in these two devices is the lower output current in bucks 1 and 2 and no support for dual phase in TPS65223.

    For more information on the PDNs and features available with the TPS6522312 please see this document.

    regards,

    Niko