Tool/software:
Hello,
so i was reading the datasheet for this component and on page 18. there is a figure 8-6 with this commentary
"Use a damping resistor R2 (~ 10 Ω) in series with C1. Equation 3 can be used to compute required C1 value for a target inrush current. A 100 kΩ resistor for R1 can be a good starting point for calculations."
R1 is the gate resistor for turning on which by this commentary is recommended 100 kOhm which seems wrong especially when you consider the R2 should be 10 Ohms - it seems that there has been a error by interchangig these two values.
In the evaulation board there is a Rg close to 10 Ohm then to 100k Ohm.
Could you clarify this value?
Thanks.