This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25176J: How many seconds until charge termination?

Part Number: BQ25176J


Tool/software:

How many seconds after the cell has reached Vrechg does it terminate charging?

I want to use this charger IC at 700mA max charge current. The load (a microcontroller) wakes for 1 second at 350mA then deep sleeps for 5 seconds at 250uA. The Iterm current is 10% of the maximum, which is 70mA. So I am concerned that the brief spike to 350mA will prevent charge termination if the deep sleep is not long enough. But if it is milliseconds, I am good.