Part Number: TPS2493
Other Parts Discussed in Thread: TPS1663, TPS2663
Tool/software:
I would like to use the basic functions. I am trying to avoid using the external soft start. IN the Start up Section, if I choose the option to not use the external soft start, the "Derated SOA/PLIM" turns red. If I use the external soft start and set "Target Fault Time" to 30ms and adjust the Actual Time Capacitance to a capacitance with a smaller capcitor than the calculated, the actual fault time is much shorter than Target Fault time and is smaller than start up time. Attached spreadsheet of calculator with my inputs.