This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: OVP FET output slew rate

Part Number: TPS6594-Q1
Other Parts Discussed in Thread: TDA4VM

Tool/software:

Hello

we use PDN-1A power solution for our product with TDA4VM, so we have TPS65941213RWERQ1 on board with the OVP protection (FET). The function is that input voltage ramps up (3.3V) then there is a delay (tVSYSOVP_INIT) and then PMIC turns on the FET by OVPGDRV pin. The FET turn on time is relatively fast which creates relatively high inrush current (our product has 5V input voltage -> 3.3V regulator -> PMIC with OVP, inrush current is 2A at 5V input in our case) which is a complication for us a bit. So I wonder if there is any possibility to change the FET turn on time (output slew rate), it means slower output ramp up, I didn't find anything in datasheet but please let me know. Thanks a lot!

Best regards

Libor