This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825: UC1825J Power output

Part Number: UC1825

Tool/software:

Hi,

We have a legacy design for lighting control using the UC1825J PWM. I have downloaded TINA and the UC1825 Transient Simulation (50W 48V to 5V Converter). I have modified the design to match our Legacy design which outputs 28V @6A. When I run the transient analysis , the output remains at 4.69V. What do I need to do to adjust the output to +28V?

thanks

Stan

slum653 (1).tsc