Other Parts Discussed in Thread: LM5155
Tool/software:
I am hoping to use the LM3488 in a boost converter for charging my batteries at 30V. Unfortunately, I only have a source that can output 20V at 3A, and the battery might draw more than that when charging. I understand that the LM3488 has a current limit feature. However, it seems like this current limit is for the maximum switched current, and not for the average current output to the load.
My questions are hence the following:
1) Is my understanding of the current limit feature correct? Or is the current limit actually for the average current output to the load.
2) If my understanding is correct, is there a part that allows me to set an output current limit, with the over current behavior being that the converter clamps the current draw, rather than shutting down.
Thank you!