Other Parts Discussed in Thread: TPS7A85
Tool/software:
Hello,
I'm upgrading a design that was using the TPS7A85 4A regulator. We will be drawing at least 3.2A per LDO, so to give some additional headroom I was thinking of switching over to the TPS7A57. Maybe not necessary, but wanted to at least simulate this new LDO.
I downloaded the PSpice for TPS7A57 and imported it into LTSpice. I setup a circuit to generate 2.4V from a 3V input. This works fine when just providing the DC voltage and doing a transient analysis.
I wanted to simulate the turn-on behavior of the LDO, so I switched my supplies to a pulse, starting from 0V. This completely kills the output. Am I doing something wrong? I tried configurations using the BIAS input instead of the charge pump, but nothing seemed to fix the behavior. Is this an issue with the model or something I'm doing? The model text says the startup behavior is modelled, so I figured I should be able to see it startup after turning on the ENABLE.
Vout seems to only respond when Vin is ramping up (and is obviously very small).
Also, the voltage on the reference pin is the 2.4V that I want on the output, and is present when I turn on the enable.
Please let me know if there is any obvious error, or an issue with the model, or maybe with how it was imported by LTSpice?
Thanks