This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: Black box function

Part Number: UCD9090A

Tool/software:

Hi Expert,

The customer uses the black box function of UCD9090A to record fault information. If rail A or rail B fails, the system will be powered off. Since the timestamp of the fault is at the second level, multiple undervoltage faults are recorded within 1 second. The customer cannot distinguish the order of the two faults from the timestamp. Any ideas to solve this issue? How long is the cycle of UCD90x fault detection? Can the order of two faults separated by 10ms be distinguished based on the order of the fault log?

Regards,
Hailiang