Tool/software:
Hello,
I use TPS26600PWPR eFuse device on a custom board.
I measured power input and GND as around 16-ohm in a failed board. Then I found that eFuse RTN-GND pins shorted directly (1-ohm), which are separated normally in the board. VIN-RTN is seen also 16-ohm. There is not any short circuit eFuse output and also eFuse device is not burned.
But after an unknown 'effect', GND-RTN is seen now shorted. What can be root cause of these result?
Best Regards,