This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2931-N: Isc (short-circuit output current) typical range not on datasheet, just that device has short-circuit protection

Part Number: LM2931-N

Tool/software:

Need Isc (short-circuit output current) typical range for fixed 5V TO-263 device -- I cannot find Isc parameter on datasheet, just a listed datasheet feature that device has short-circuit protection.

  • Hi Brett,

    I couldn't find it either. I can order some of these devices and test them on an EVM for the typical current limit. Can you confirm the correct part number? There are a few 5-V options in the TO-263 package. 

    Regards,

    Nick