This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: Input current limit

Part Number: BQ25895


Tool/software:

Hi, 

A couple questions - I was reading through some of the older posts and was a bit confused about the input current limit and what to appropriately set it to. Some posts made me think it was the lower limit? which is a bit confusing and i just wanted to verify. 

Context I have a custom PCB with two 18650 batteries, a solar panel (supplies ~500ma) and a USBC to charge the batteries as well. We are setting the USBC up to provide 3A. Mosfet will switch from solar charging to USBC when plugged in

1. If i'm using a USBC for charging and a solar panel what should I set the input current limit to? 

2. Would it be able to support the solar panel for charging as well if the current is much lower than the expected USBC input current?

Thank you!