Other Parts Discussed in Thread: BQ51013
Tool/software:
I am troubleshooting the same problem that is described in the related/linked forum post: "BQ51013B: Prioritized wireless charging".
It seems that when I have EN2 pulled high and EN1 pulled low (utilizing the internal 200K pulldown) the wireless charging is allowed, but the adapter charging is never allowed even when the the wireless TX is not present.
This manifests itself as #AD_EN remaining HIGH regardless of whether the wireless charger is present.
When EN2 and EN1 are both low, the handoff between wireless and adapter charging are as described in the datasheet.
This part does appear to be behaving like the BQ51013 instead of the BQ51013B as described in the "related" post. (I double checked the marking on my part and it is labeled as BQ51013B).
Any additional thoughts on this issue would be helpful.
Thanks.