Other Parts Discussed in Thread: TPS7A39
Tool/software:
I am designing a split ±1.65V power supply with a maximum current output of 40 mA to power two op-amps. I could also work with more standard output values such as +-1.5V or +-1.8V. The input voltage is 3.3V. I have identified the TPS7A05 as a potential candidate for generating the positive voltage. Is this a suitable choice?
Additionally, what IC would you recommend for generating the negative voltage? Is there a single IC that can provide both positive and negative voltage outputs?