Tool/software:
Hello, and thank you in advance for your help.
We are trying to build a system capable of charging a Samsung tablet with a PD port while still being a UFP. We could not achieve this by configuring CC resistors via hardware, as the tablet, as soon as it gets connected, takes on the role of UFP Sink, and we can’t get the communication working. So I guess there is no other option than using a PD controller on our board to perform a data role swap.
Our system will not deliver more than 10W to the tablet, and once the sourcing device role is implemented, it will not need to change its role or deliver more power than anticipated. Therefore, we need the simplest PD controller possible to achieve this.
Do you recommend the TPS26750 for this application, or is there a simpler option for this use case?
Best regards,
Francisco