This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: OCVGD,OCVFAIL and OCVCOMP fields never changing when reading in battery status flags

Part Number: BQ27220

Tool/software:

When I read the battery status register I can see the OCV_GOOD and OCV_COMP indicators are always 1 and are never going low, as if there was no new OCV request during gauge runtime

Sleep cycle period is configured to 20s. 

Gauge is currently in UNSEALED mode and here are the regs content when I read RAM conf and registers:

Battery Status Flags=4268
DSG:0 SYSDWN:0 TDA:0 BATTPRES:1 AUTH_GD:0 OCVGD:1 TCA:1 CHGINH:0 FC:1 OTD:0 OTC:0 SLEEP:0 OCVFAIL:0 OCVCOMP:1 FD:0

Operating Status Flags= b4
CALMD:0 SEC:2 EDV2:0 VDQ:1 INITCOMP:1 SMTH:0 BTPINT:1  CFGUPDATE:0

Gauging Status Flags=804a
FD:0 FC:1 TD:0 TC:1 EDV:0 DSG:1 CF:0 FCCX:0 EDV1:0 EDV2:0 VDQ:1

GAUGE_CONF: raw=102a
CCT=0 CSYNC=1 EDV_CMP=1 SC=0 FIXED_EDV0=1 FCC_LIM=0 FC_FOR_VDQ=0 IGNORE_SD=0 SME0=1

1) Do I have to switch to SEAL mode to have automatic OCV read done by gauge during sleep cycle ?

2) Do I have to change something in config ?

3) Do I have to assert some bit in some register to clear the OCV_FAIL/GOOD/DONE status ?

Regards