This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25622E: VREG minimum

Part Number: BQ25622E


Tool/software:

For BQ25622E, the VREG battery voltage charge threshold is settable from 3.5V ~ 4.8V according to the datasheet.

When in PREWARM temp range, the VREG can be adjusted from VREG-100mV to VREG-300mV with the TS_VSET_PREWARM reg.

Does this all work properly at lowest VREG setting? i.e. if we set VREG=3.5V and then enter PREWARM state with VREG-300mV, will the batt VREG drop and properly regulate to 3.2V?

  • Hi Peter, 

    Yes, VREG can be properly regulated to 3.2V when in PREWARM temperature range with VREG = 3.5V and TS_VSET_PREWARM = VREG-300mV.  Please be aware VSYSMIN setting must be reduced to a value less than 3.2V to allow the device to terminate charge properly. 

    Best Regards,

    Garrett