Tool/software:
Hi team,
How can customer clear dead-battery flag? There are description on 8.3.2 Power Management, 8.3.6 Default Behavior Configuration (ADCIN1, ADCIN2), 9.3.1.1 VIN_3V3 Input Switch.
Fundamentally, the device needs to be supplied from VIN_3V3? I assume this is sink-only device and it can be used without VIN_3V3 and supplied from VBUS through LDO in all cases. Is that correct?
If there is 3.3V supply into VIN_3V3, is there any merit for the device?
Regards,
Hayashi