Tool/software:
Hi,
How to configure ucc28950 ic work in open loop condtion for test purpose
we have to generate output pulse without any feed back loop
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nithin,
To run UCC28950 in open loop, connect EA- and COMP pins together. The error amplifier output now tracks the voltage at EA+ in voltage follower configuration. Apply a voltage at EA+ starting with 0V, and slowly increasing should help provide open loop operation.
If you have any related question, click on 'Ask related question'. If you have a new question, use 'Ask a new question' option.
Regards
Hemanth
Nithin,
Please connect the control circuit components per the requirements and following datasheet including the frequency setting, you need.
Recommend to use 15kohm for DELAB, DELCD, DELEF and ADELEF to GND. RSUM connecting to VREF makes the controller work in voltage mode control
Please refer UCC2895x-Q1 Automotive Phase-Shifted Full-Bridge Controller for Wide-Input Voltage Range Applications datasheet (Rev. C) for more details.
Regards
Hemanth
Nithin,
Did you go through each pin functionality in the datasheet?
Can you measure all the pin voltages, that should help you debugging the circuit having understood each pin functionality and expected voltage.
Please use all 4 or 8 channels to see them in sync.
Regards
Hemanth
Nithin,
"EA pin and COM i have given below"
Are you applying any voltage at COMP pin directly?
Regards
Hemanth
Nithin,
Just to re-iterate and for future reference on this thread, voltage shall not be applied at COMP pin directly. As mentioned before the EA should operate in voltage follower mode.
Hope the issue got resolved as I don't see further discussion for about two weeks. Closing the thread.
If you have a related question click on 'Ask a related question' and click on 'Ask a new question' otherwise.
Regards
Hemanth