Part Number: UC3843A
Other Parts Discussed in Thread: TL431
Tool/software:
Good morning
Is there an Application Note or a White Paper that addresses the topic "how to reduce the oscillation frequency of the UC384x family PWM controllers as the duty cycle decreases"?
Reason: I'm sizing a flyback without PFC preregulator due to space & cost (total requirements: Vin = 85-269Vac 47-63Hz; Vout = 30-95Vdc under uC control by DAC output, Pout = 10-180W variable under load needs, Poutmax,avg = 150W for thermal purposes; Ioutmax = 1.9A, Ioutmax,avg = 1.6A for thermal purposes), it would be interesting to be able to vary the switching frequency in a 1:2 range from minimum duty cycle to maximum duty cycle in order to have sense currents and ON times that are not very small even in very bad conditions (example: Vin = 269Vac, Pout = 10W).
Thank you for the information and references you want to give me.
Greetings
Marco