This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808: reset duration

Part Number: TPS3808
Other Parts Discussed in Thread: , TPS3842

Tool/software:


Hello,
I am designing and testing reset signal circuit using TPS3808.
The reset time is approximately 9.5sec.
So I connect 1,65uF +/-10% capacitor to CT pin of TPS3808.

The reset duration measurement result on prototype circuit is approximately 8sec.
An error of approximately 1.5 second was confirmed in the reset duration.


I would like to confirm whether this level of error actually occurs.
(I guess that the cause is a current error of the internal 220nA current source)

Regards, MESH