Part Number: BQ25750
Tool/software:
Hello TI team.
I have a question about ILIM concept and setting.
For example,
- ILIM_HIZ pin setting is 5A
- ICHG pin setting is 1A
- System current consumption is ~20A
In this case, if I connect external input source(power adapter able to supply 20A, no battery charging state, only operating system load 20A),
Does the Charger is pass maximum 5A and blocking the rest input power by ILIM set?
Thank you.