This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38015: when 48V plug in that will any impact?

Part Number: LMR38015

Tool/software:

Hi team.

when 48V plug in directlly  that will any impact? No use hotswap solution.

Need add some RC filter to prevent spike?

  • Hi Jimmy,

    This is a hot-plug scenario so you will want to monitor the vin pin (using a scope probe) to make sure the transients don't exceed 80V operating voltage. You may need to add a TVS diode at the input that clamps at 85V (abs max) or lower to prevent damage to IC.

    Cheers,

    Richard