Other Parts Discussed in Thread: TPS25980, TPS25983, TPS1663, TPS2663
Tool/software:
Hi
Could you help recommend E-FUSE or Ideal Diode products
Device Input Input Power: 24V , Current: 5A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
I am suggesting from eFuse portfolio (integrated FET)
TPS25980 is one option but its max recommended voltage is 24V/8A. If you need some buffer, better to use TPS25983 which is p2p device with 26V/20A capability.
Another option is TPS1663/TPS2663 which are 60V/6A device.
Best Regards,
Arush
Hi Gareth,
It looks like your application will require reverse current blocking. Out of all the suggested options above, only TPS2663 can support RCB + 24V/5A operating conditions.
Please let me know if you need ideal diode. I will have to add my colleague who is expert in those.
Best Regards,
Arush