This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62290-Q1: TPS62290TDRVRQ1

Part Number: TPS62290-Q1


Tool/software:

Cff colaps every time we put a diaplsy on the 5vdc input that feeds the TSP

  • Hello,

    The question/issue is not clear to me. Please provide the schematic, layout and scope plots to explain the problem.

    Thanks,

    Febin

  • Please note the voltage drop when connecting the display

    display is max 250 mA, the PSU is 1A

    Do you recognise theeffect?

  • We designed the diagram from TI includung the right lay-out

  • Hello Anton,

    Thanks for the video file. However, which voltage is this? Is it Vout?

    I would need the schematic to understand better.

    I need to see scope plots for Vin, Vout, Vsw, Load current/inductor current to start with.

    Thanks,

    Febin

  • the video 

  • 0552.storing 3V3 circuit.pdf

    Hi Febin

    See attsached.

    Regards

    Anton

  • Hi Anton,

    Thanks for sharing the files. The problem description is clear. 

    I have a couple of questions:

    - What is the CPU load? I assume the display load ~250 mA is in addition to the CPU load.

    Would you be able to capture the Inductor current at this point when the display is active.

    - I assume there is no other device connected to this 3.3V rail except the CPU and display.

    - Another thought, could there be any possibility of undamped input filter in this case? Have you tried to test without the input filter?

    - Would you be able to share the layout with us?

    Thanks, 

    Febin

  • Hi Anton,

    Please also share the complete schematic and layout showing the load to the TPS62290-Q1.

    Please also clarify your exact measurement points for Vin, Vout.

    Thanks, 

    Febin