This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: Priority Power MUX Design for 24-36V, 10A – Need Reference Schematic

Part Number: LM7480-Q1

Tool/software:

Hello,

We are designing a Priority Power MUX for a 24-36V input with a 10A rating and need guidance on implementation. Our requirements:

  1. Primary (Power Adapter) should be selected when both inputs are available.
  2. Secondary (Battery) should be used only if the Primary is unavailable.
  3. Seamless switching with minimal voltage drop is preferred.

Could you suggest the best approach? Additionally, if you have a reference schematic to achieve this design, it would be very helpful.

Thanks in advance!

Regards,
Sivam Natesan