This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ644A2-Q1: FB tolerance

Part Number: LMQ644A2-Q1

Tool/software:

Hi team,

Could you please advise the tolerance of fb pin at 3.3V and 5V fixed?

It is described as below in the top page of the datasheet, but Vfb1/2, Vfb_so is specified as min/max 1.5% in EE table for adjustable. 

So I would like to double check if 1% or 1.5% is correct. 

"1% accurate fixed 3.3V, 5V or adjustable
outputs from 0.8V to 20V"

regards,