Other Parts Discussed in Thread: TL431
Tool/software:
Hello all together,
I want to build a flyback converter reference design (In: 200-1000VDC, Out: 24VDC 1.5A). I don't have much experience in flyback converters. So I created Designs with TI Webbench. I selected a Design using UCC28C58DR. I recalculated according the datasheet and build up the design with some little changes.
First Test showed that the design is working but was unstable. So I had to change the compensation to get stable PWM cycles. Efficiency Testing showed expected peek perfomance but the curves are somehow confusing with some ups and downs.
I was looking at the PWM signal at the source pin of the switcher to check operating modes of the controller. At 200V Input Voltage the design is working in CCM Mode with round about 60% PWM at full load. When lowering the load, it transitions into DCM Mode and then at light loads it stucks around 30% PWM. Further lowering the load leads to blanking of full PWM cycles. Output remains stable at 24V for the whole load range.
I'm confused about why PWM stucks at 30% and is not lowering further with decreasing load? I'm also confused about the feedback path in the design. According to the webbench I connected it to the Fb Pin of the controller. I thought it should also be possible connecting it to the comp pin with FB tied to GND. Because the error amplifier is made by the TL431 in the feedback path?SiC_Flyback_001.pdfWBDesign200to1000V_Diode.pdf