Tool/software:
Dear Team,
My customer is considering to use the TPS65640. The tolerance of VGH of Boost Converter 2 is +/-3%. However, this tolerance does not meet the LCD panel requirements.
- TPS65640 Boost Converter 2 VGH:
- Output voltage range: 15V to 37V
- Tolerance: -3% to +3%
- LCD Panel VGH requirement:
- 18.2V ~ 18.7V ~ 19.2V
- +/-2.7%
Do you have the VGH distribution characteristics data?
Best Regards,
Koshi Ninomiya