Other Parts Discussed in Thread: TPS922051
Tool/software:
We have a project requirement of Double horn flood light camera with PIR sensor. Image of project is attached.
In this project we have two horns containing array of white LEDs. We need solution for this LED driver also it should include support of dimming from some microcontroller PWM pin. We have checked power integrity portfolio and found reference design "DER-657 - 45 W High Power Factor, Isolated Fly back with Switched Valley Fill PFC LED Driver" but this design doesn't include any dimming support. Requirement for LED driver is 120Vac/240Vac 50/60Hz input and output is 80V/580mA dimmable .
Can we have suggestion on above requirement?
Along with above design can we use single fly-back transformer to generate dimmable supply for LEDs and 5V/3Amp supply for MCU section? If that's possible then please suggest the reference design and part as well.