This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: Failure of TI Part BQ7791501

Part Number: BQ77915

Tool/software:

Dear TI Expert,

Attached documents as follow

1. Circuit Schematic (Please Refer to attached document. The cell configuration of Both IC (3+3), (4+4) and (5+5).

2. IC Part No: BQ7791501

We had made 3000 Nos. BMS in which so many IC is failed. Application is small resistive load and 5-10A inductive load & Lighting Load.

Due to high failure, Customer is not accepting our BMS.

We are unable to analyze the reason of failure.

(Additional Information, when the same circuit use for LFP (BQ7791514), The failure rate is very low.

Thanks 

Rahul Sharma

Lithion Power Private Limited

I10_20A_V1.0.pdf