Tool/software:
Hi,
I have some trouble understanding the tolerance of the OV pin of TPS4800-Q1 (voltage rising threshold).
Could you please clarify?
In the datasheet (12/2024 version), there are two different values given.
on page 6: Overvoltage threshold input, rising: 1.171V (min) 1.225V (typ) 1.278V (max)
-> which is -4.41% / +4.33%
on page 19 (chapter 7.3.4): "an accurate overvoltage protection (< ±2%)"
Obviously, this is a big difference and in our application we require a tight tolerance.
Does this difference relate to the operating conditions (temperature)?
i.e. -4.41% / +4.33% from -40°C to +125°C and ±2% at 25°C ?
If so, could you please provide more data to the min/max values for a reduced temperature range (0°C - 85°C) ?
Kind regards,
Matthias Zimmermann