Tool/software:
Hello, I have designed a buck converter circuit using LM5085MY/NOPB for 5V 10A output. The input voltage voltage range is between 12V-30V.
The circuit is working fine for input voltage range 12-18V and giving stable 5V output.
When input is between 19V- 24V the output drops to 4V which is unexpected.
If i increase input voltage between 24V-30V, output increases to 5V.
In short,
For 12V-18V input - 5V output.
For 19V-24V input- ~4V output.
For 25-30V input- 5V output.
I require constant 5V output which can able to handle load of up to 10A.
I'm sharing circuit for reference. thanks in advance.