Part Number: UCC27211A-Q1
Tool/software:
I am comparing RevA and RevB of the UCC27211A-Q1 datasheet.
Q1: 5.4 Thermal Information has changed. Is this due to PCN# 20240723008.2? (PCN adds AIZU along with DFAB)
- If yes, how has it been affected?
- If no, please tell me why it has changed.
Q2: The operating junction temperature for RevA is +150°C. For RevB, it is +140°C.
Is it possible to make it 150°C?