This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65132S: About operation of disable status

Part Number: TPS65132S


Tool/software:

Hi team,

Our customer tested this device and observed both of ±5V output voltage increase up to 0.8V when other IO supply (1.8V) start up in start up sequence when EN is Low.

The device condition is below,

Input voltage :5V

Output voltage :±5V

Output current  : 80mA(+5V), 60mA(-5V)

In this case, if input voltage is below output voltage when EN is Low, is it possible to occure reverse current to input?

Or are there any possibility of any device abnomal operation?  

Best regards,

teritama