This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923653: Any issue with dimming when max output current is only 100mA?

Part Number: TPS923653


Tool/software:

Looking at the dimming ratios in the datasheet, is there any issue hitting the 1M:1 dimming ratio when the max string current is only 100mA?

Thanks! 

  • Hi Cameron,

    It is very hard to achieve the 1M:1 dimming ratio with good linearity when max output current is only 100mA. The CSN pin leakage current, the leakage current through OVP resistor divider and other non-ideal factors will make the linearity very poor at low-brightness condition.

    Best Regards,

    Steven