Tool/software:
I am wanting to perform a resistance measurement between the output of the TPS746-Q1 and ground to verify that there are no shorts before turning on power. The block diagram shows 2 internal resistors in series between the output pin and ground. Can you provide the values of these resistors for the 1.8V and 1.0V fixed voltage versions of the part?