This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Chemistry Tab not available in BQ Studio

Part Number: BQ34110
Other Parts Discussed in Thread: EV2400

Tool/software:

I am using EV2400 to calibrate my BQ34110. I have tried with three BQ STUDIO versions 1.3.54, 1.3.86 and 1.3.101. I am able to detect the IC and monitor the voltage and current. But I am using a Lead Acid Battery 12v 1.3Ah. As the default chemistry is Single cell series Li-ion I guess. I am unable to find the chemistry tab to change the chemistry. Also even after sending the unseal command, I am unable to change the series of cells and Pin control config parameters.