Other Parts Discussed in Thread: UCC28951, UCC28950
Tool/software:
Hello..
I am planning to design an SMPS with the following specifications using the master-slave method of UCC28951.
-. Specifications
INPUT: DC 350V ~ DC 420V
OUTPUT: DC 52V 1,500kW (approximately 289A)
-. Questions are as follows.
1. Can UCC28951 operate as one master and a maximum of how many slaves?
2. If there are design reference documents and design data (design files and PDF files, etc.) for the master-slave method of UCC28951, please share them.
4. If there are design reference documents and design data (design files and PDF files, etc.) for synchronous rectification when configuring the output as a current doubler method, please share them.
Thank you.