Other Parts Discussed in Thread: TL431
Tool/software:
Hi,
I have SMPS project , where I have 6.5V @ 1.5A output as shown in the figure below:

However, the output with full load (around 1.3A) has this behavior as shown in the figure:

Do I need to change the capacitors (C13 and C15), is there any calculation? Or will I need to change other chip parameters?
What is the best way to proceed in this situation?