This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: FETS in parallel

Part Number: BQ77915


Tool/software:

Hello

 i want to use the following N-Channel mosfet for the CHG FET and DSG FET: 

- Part nummber: BSC070N10LS5ATMA1

- (Qg) (Max.) = 20 nC @ 4.5 V

- 7mOhm at 40A, 10V

My question is, how many of these FETS i can put in parallel (for heat dissipation etc.) without pulling to much energy from the CHG an DSG drivers of the Chip? 

Can i put 4 of them in parallel? (So 4 in parallel for CHG driver and 4 in parallel for DSG driver)

Thanks

Silvan